DQS configuration for MPC8349EA (DQS_CFG field)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

DQS configuration for MPC8349EA (DQS_CFG field)

跳至解决方案
939 次查看
mallik
Contributor II

Hi,

MPC8349EA has single ended strobe MDQS[0-8].

But the reference manual Table 13, Pg 385

says, DQS can be configured for Either Differential or single ended signal.

Whether we can configure DQS as Differential in MPC8349EA-667Mhz

标签 (1)
标记 (1)
1 解答
728 次查看
Bulat
NXP Employee
NXP Employee

It is a mistake in the manual that has been already fixed. Please take a look at the manual errata (MPC8349EARMAD), it states:

"9.4.1.8, 9-23 Changed setting 01 of DDR_SDRAM_CONFIG_2[DQS_CFG] to reserved."

So no, differential DQS is not available and can not be configured in the MPC8349.

在原帖中查看解决方案

1 回复
729 次查看
Bulat
NXP Employee
NXP Employee

It is a mistake in the manual that has been already fixed. Please take a look at the manual errata (MPC8349EARMAD), it states:

"9.4.1.8, 9-23 Changed setting 01 of DDR_SDRAM_CONFIG_2[DQS_CFG] to reserved."

So no, differential DQS is not available and can not be configured in the MPC8349.