Boot flash signals

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Boot flash signals

665件の閲覧回数
barcelona_fan
Contributor II

Hello,

I'm trying to design a proper PCB which my MPC8280 will sit on, i can't manage to find the proper way to wire  my BOOT Flash in the reference manual. if the relevant memory controller is Memory controller 0 that is used for the boot flash, i can't seem to find what are the selected Address and Data pins used to talk to the Flash on startup? If port size matters then i'm planning on 8 bit port size, which means 22 pins of address and 8 bits of data bus. 

Any help is appreciated, i seem to get confused in the datasheet. 

Thanks a bunch!

0 件の賞賛
返信
1 返信

623件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please refer to the PQ2FADS-ZU schematics (connection of the U52):

https://www.nxp.com/downloads/en/schematics/PQ2FADSZUSCH.zip 

0 件の賞賛
返信