i.MX 7Dual power sequence measurement

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX 7Dual power sequence measurement

1,323件の閲覧回数
justin_hsieh
Contributor I

Dear Team,

According i.MX 7Dual datasheet, it shows timing spec. as below,

T1 Time from SVNS power stable to other power rails start to ramp, minimal delay is 2ms,
no max delay requirement.

sequence.png

Can you kindly clearify T1 means that 90%*VDD_SNVS_IN to 10%*NVCCGPIO or 90%*NVCCGPIO?

Thanks, 

ラベル(2)
0 件の賞賛
返信
1 返信

1,232件の閲覧回数
art
NXP Employee
NXP Employee

Here T1 means 90% VDD_SNVS_IN to 10% NVCCGPIO and other voltages except of NVCC_DRAM and NVCC_DRAM_CKE.

Best Regards,
Artur

0 件の賞賛
返信