What are the differences between the PWM & PFM & auto skip mode on FS5600 PMIC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What are the differences between the PWM & PFM & auto skip mode on FS5600 PMIC?

2,383 Views
shafers
Contributor I

What are the differences between the PWM & PFM & autoskip mode(SW mode) on FS5600 PMIC?

which one is more friendly for EMC performance?

Thanks

BR

Shafers

0 Kudos
Reply
1 Reply

2,375 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Louis,

the PWM keeps the same frequency of the waveform and changes the duty cycle, to change the power transferred, while the PFM modulation keeps the same duty cycle and changes the frequency to change the transferred power. 

JozefKozon_0-1692184721946.png

JozefKozon_1-1692184924554.png

In skip mode some of the pulses are skipped to lower the power transferred. 

JozefKozon_3-1692185147338.png

Regarding the EMC, the skip mode is the worse for the EMC to other devices. For the PWM and PFM, its not that easy to answer. It depends on many aspects. Please check a quote below.

JozefKozon_2-1692185114309.png

With Best Regards,

Jozef

 

 

0 Kudos
Reply