PMIC PF8100 doesn't start, V1P5A problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PMIC PF8100 doesn't start, V1P5A problem

Jump to solution
2,295 Views
iderzh
Contributor II

Hello,

My design has PF8100XXES PMIC  with i.MX8QXP SoC.

The PMIC doesn't start - LDO1 and LDO2 shows 0V, 4.0V is supplied  to VIN and LDO12IN.

When V1P5D rises to 1.5V the V1P5A rises to 1.5V and immediately falls to 0V (see attached picture V1P5D -yan, V1P5A - red).

The schematics attached as well.

Regards,

Igor

Labels (2)
1 Solution
2,013 Views
iderzh
Contributor II

Hello Jose,

Thank you for reply!

There were two problems in my design:

1. Unassembled INT# PU 1.8V (R490 - 100K).

2. My P8100 wasn't OTP programmed, so I should been use default hardwire configuration VDDOTP PU 1.5V (R365 - 10K, R366 -DNP).

Best Regards,

Igor

pmic8100_solution.png

View solution in original post

3 Replies
2,013 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

 

First, you should know the device ID, as the PN is PF8100XXES, it is customer sample. So you need to know the OTP configuration of the device you use. We recommend you to use CC version PF8100 to supply i.MX8QXP platform.

 

Seems like VSNVS is not power up in your test result, so PWRON can't be pulled up and PMIC isn't turn on. It should be 3.0V when VIn is high. 

Try to use 5V VIN and Confirm VSNVS is power on in PF8100 OTP configuration. 

 

Do you mind sharing the following information, please?

  1. Customer Name:
  2. Customer website:
  3. Market Segment:
    4. Project Name:
    5. End Product/ Product:
    6. Project Stage:
    7. Annual Production Volume:
    8. Project Details:
    9. Prod Start Date:


Have a great day,
Jose

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

2,014 Views
iderzh
Contributor II

Hello Jose,

Thank you for reply!

There were two problems in my design:

1. Unassembled INT# PU 1.8V (R490 - 100K).

2. My P8100 wasn't OTP programmed, so I should been use default hardwire configuration VDDOTP PU 1.5V (R365 - 10K, R366 -DNP).

Best Regards,

Igor

pmic8100_solution.png

2,013 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Igor,

Please share the following information:

  1. Customer Name:
  2. Customer website:
  3. Market Segment:
  4. Project Name:
  5. End Product/ Product:
  6. Project Stage:
  7. Annual Production Volume:
  8. Project Details:
  9. Prod Start Date:


Have a great day,
Jose

0 Kudos