A customer wants to power some LEDs from VSYS.
1) Is it OK to do this?
2) I assume the max current they could take would be the current taken would be dictated by the current limit setting for the Front-end LDO minus the current taken from the LDO/Switchers on the PF1510.
Thanks
Mark
解決済! 解決策の投稿を見る。
Hi Mark,
Yes, you can power some LEDs from VSYS power rail from the PF1510.
You are correct, the max current they could take is dictated by the current limit setting for the Front-end LDO minus the current taken from the LDO/Switchers on the PF1510.
Regards,
Jose Reyes
Hi Mark,
Yes, you can power some LEDs from VSYS power rail from the PF1510.
You are correct, the max current they could take is dictated by the current limit setting for the Front-end LDO minus the current taken from the LDO/Switchers on the PF1510.
Regards,
Jose Reyes
Also Can we connect 5V to Vin of PF1510 and use Vsys to power input of all the switchers and LDO of PMIC and also use Vsys to provide some pull ups on the boards?