A customer wants to power some LEDs from VSYS.
1) Is it OK to do this?
2) I assume the max current they could take would be the current taken would be dictated by the current limit setting for the Front-end LDO minus the current taken from the LDO/Switchers on the PF1510.
Thanks
Mark
已解决! 转到解答。
Hi Mark,
Yes, you can power some LEDs from VSYS power rail from the PF1510.
You are correct, the max current they could take is dictated by the current limit setting for the Front-end LDO minus the current taken from the LDO/Switchers on the PF1510.
Regards,
Jose Reyes
Hi Mark,
Yes, you can power some LEDs from VSYS power rail from the PF1510.
You are correct, the max current they could take is dictated by the current limit setting for the Front-end LDO minus the current taken from the LDO/Switchers on the PF1510.
Regards,
Jose Reyes