Meaning of MWCT1000 "Device Fault 0x400"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Meaning of MWCT1000 "Device Fault 0x400"

718 Views
mwmerlo
Contributor I

We are debugging a custom board that uses the MWCT1000 wireless power Tx and we are encountering a Device Fault 0x400 reported in the NXP provided Freemaster project. Specifically, RunTimeParams[0].wDeviceFaultStatus = 0x400 during the fault condition.  We have gone through the source code but it appears this fault condition is set within the binary library provided by NXP and therefore we cannot view this part of the code. We have done a lot of testing to try to determine the meaning of this fault code without much luck. I can go into the details of this testing if needed, but the short question is:

Does anyone know the meaning of Device Fault = 0x400?

Thanks,
Mark

0 Kudos
1 Reply

96 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Please check the definition as below, which is in systemProtection.c file:

xiangjun_rong_0-1712633851351.png

 

Customer can also log in NXP website, download the users reference manual and lib reference manual, which have the detail description of the variables, thanks!

BR

XiangJun Rong

0 Kudos