Junction temperature of NTS0104

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Junction temperature of NTS0104

3,076 Views
nxf64834
NXP Employee
NXP Employee

Can someone please let me know the Junction temperature of NTS0104?

It is not provided in the datasheet.

 

Thanks in advance!!

0 Kudos
Reply
6 Replies

3,068 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

Please confirm which version of the NTS0104 you are interested in, there are 7 different part numbers with 4 different packages associated with the NTS0104.

I need this information to search for the Junction Temperature data.

Thanks,

Jose

0 Kudos
Reply

3,065 Views
nxf64834
NXP Employee
NXP Employee

Hi, 

I need this data for NTS0104PW-Q100.

Thanks

0 Kudos
Reply

3,063 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

Here is the NTS0104PW-Q100 information page (https://www.nxp.com/part/NTS0104PW-Q100#/), if you scroll down, you will find a table of the Operating Characteristics, in this table you can find:

Rth(j-a) (K/W) = 175  (Junction to ambient)

th(j-top) (K/W) = 40 (Junction to top)

 

Is this the information you are looking for?

 

reyes_0-1613408592720.png

Regards,

Jose

0 Kudos
Reply

3,043 Views
nxf64834
NXP Employee
NXP Employee

Hi,

The info that you are indicating to is for thermal resistance. What I am looking for is Maximum Junction temperature just like it is clearly provided in the datasheet of NTS0304(attached pic). 

Thanks

0 Kudos
Reply

3,030 Views
reyes
NXP TechSupport
NXP TechSupport

I will check with QA and get back to you

0 Kudos
Reply

3,021 Views
nxf64834
NXP Employee
NXP Employee

Thanks. That would be great.

Also, there is one more doubt, the maximum junction temperature of NTS0304 is mentioned 85 degree C in datasheet, whereas the maximum ambient temperature given is 125 degree C.

According to formula of Junction temp, it is equal to the summation of Ambient temperature and product of Thermal resistance & Power dissipation. Hence, Junction temp will always be greater than ambient temp.

My query is if we are using the IC at 100 degree ambient temp, then the junction temp will be greater than 100 degree C, hence crossing the maximum junction temperature but the ambient is within the limits. So, can we use this IC at 100 degree C?

0 Kudos
Reply