In FS6513C SBC, deep fail safe state is for the device or the 2 machines(MSM & FSSM) individually?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

In FS6513C SBC, deep fail safe state is for the device or the 2 machines(MSM & FSSM) individually?

1,908 Views
vaibhav_sharma
Contributor III

According to FS6500 SBC user manual, when the deep fail-safe function is enabled, as soon as either the fault error counter reaches its final value or the RSTB pin remains
asserted low for more than 8.0 s, the device switches all the regulators off (except VKAM if VKAM was on) and maintain the safe stateSBC (FS0B and FS1B are activated). So the device enters Deep fail-safe state or is it a state for the machines in(MSM & FSSM) individually, because there are separate bits for checking the deep fail-safe enable/disable state for both the machines?

Thanks in advance.

Labels (2)
0 Kudos
4 Replies

1,552 Views
vaibhav_sharma
Contributor III

Hi Paulina,

Please reply. 

0 Kudos

1,552 Views
lisettelozano
NXP Employee
NXP Employee

 Hello Vaibhav,

Basically yes. When the deep fail-state feature is enabled and after the fault error counter reaches its final value or the RESET pin remains asserted low for more than 8 seconds, the device modes to the deep fail-state and will maintain the system in a safe state system (Fail-safe state machine; FS0B and FS1B are activated). Only a Key_OFF/Key_ON sequence (IO_0 = 0 followed by IO_0 = 1) at the system level can recover the situation.

I apologize for the delayed response. 

Have a great day, 

Paulina

1,552 Views
lisettelozano
NXP Employee
NXP Employee

Hello Vaibhav,

The device has two state machines work in parallel: the main state machine which controls the power management and the fail-safe state machine which controls all the safety features (WD, RSTB, FS0B, FS1B, ...). When the deep fail-safe feature is enabled, the SBC completely switched the MCU off and maintains the system in the fail-safe state (FS0B and FS1B are activated).

I hope this information can be helpful. 


Have a great day,

Paulina

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

1,552 Views
vaibhav_sharma
Contributor III

Hi Paulina, 

Thanks for the response.

So is it possible that only one of the state machine goes into deep fail safe state (as they are isolated state machines working in parallel)? & the other keeps working fine.

0 Kudos