How to know the coil cell is charged in PF3001

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to know the coil cell is charged in PF3001

2,434件の閲覧回数
bin_lei
Contributor I

We had used the coin-cell charger in PF3001, we want to indicate it by LED when the coil-cell is charging or is charged, but how to know the coil cell is charging or is charged?  Thank you.

ラベル(1)
0 件の賞賛
返信
6 返答(返信)

2,314件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi

I have concept below if you are interest in it you could try:

1: Set the charge voltage(VCOIN (V)) such as 3V.

2: Connect the VCOIN (V) line from your board with voltage comparator input port , also connect  reference voltage 3V to comparator other port.

3: If actual VCOIN is above setting value(3V),there is output signal on comparator ,this signal high or low level also can be showed in LED output.

0 件の賞賛
返信

2,314件の閲覧回数
bin_lei
Contributor I

Thank you. That will be added a comparator, can I used the ADC pin in IMX6UL for this function?

0 件の賞賛
返信

2,314件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Please show me more information,if use ADC then what to do next?

0 件の賞賛
返信

2,314件の閲覧回数
bin_lei
Contributor I

We plan to do like this: read the ADC pin and compared it with 2V/3.1V by software, if it is less than 2V, enable the charger, indicate it is charging with a LED by a GPIO. If it is more than 3.1 disable the charger, indicate it is charged with a LED by a GPIO. Is it feasible?

0 件の賞賛
返信

2,314件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Yes,it's feasible.

2,314件の閲覧回数
bin_lei
Contributor I

Got it. Thanks.

0 件の賞賛
返信