How to control H/L output for the IO_4 of FS65

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to control H/L output for the IO_4 of FS65

585 Views
hsieh_jaros
Contributor I

Hi NXP

I want to control the io_4 for H/L with output  and to setting the register (0x17 ; IO_OUT_AMUX) by SPI

 The Sending command is 0xACE0 for register 0x17 by  SPI TX and get RX data is 0x8700

(Yellow line is MISO of SPI and  Green line is MOSI of SPI)

IMG_20200515_143039.jpg

and then I check the data of register 0x17,the the setting still is 0 for "IO_OUT_4_EN" and "IO_OUT_4" of register 0x17 (IO_OUT_AMUX)。

So 

How to control H/L output for the IO_4 of FS65 ?

0 Kudos
1 Reply

554 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

I test this function in EVB successfully,step setting below:

1: Configure it in debug mode

2: Enter into normal mode

3:directly setting IO_OUT_AMUX register bit 6-7 as '11'

4: jumper 21 setting to connect PIN3 with PIN2 then LED-D10 state is ON.

5: setting IO_OUT_AMUX register bit 6-7 as '01' then the LED-D10 is OFF.

You can download the EVB schematic or other information below:

KITFS4503CAEEVM | Evaluation Board for FS4500 | NXP 

0 Kudos