FS6520 VAUX for 5V no output

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS6520 VAUX for 5V no output

Jump to solution
1,444 Views
LyncLin
Contributor III

Hi NXP team,

 

I have an issue with FS6520 VAUX output that need your help.  The hardware schametics are attached.

The select pin-31 is connected a 24 kohm resistor. The DEBUG mode is enabled by connecting Pin-15 DEBUG to a voltage divided from VPRE 6.5V. SW_CORE is confirmed to output around 1.25V.

VCCA and VAUX are both connected to an external PNP transistor (BCP52-16,115). On output of VCCA, an 3.28V output voltage can be measured on Pin-43 VCCA, and it's around 5.9V on VCCA_B and 6.6V on VCCA_E. However, on pin-38 VAUX, it's close to 0V, and it's around 7.8V on VAUX_B and 8.2V on VAUX_E.It looks FS0B is also pulled down LOW.

Currently there's no SPI or software available. It will be appreciated if you can provide any suggestions to debug this issue. Thanks a lot in advance!

Regards,

Lync

LyncLin_0-1694441374128.png

LyncLin_1-1694441404703.png

LyncLin_2-1694441425842.png

LyncLin_3-1694441453284.png

 

 

Labels (2)
Tags (2)
0 Kudos
Reply
1 Solution
1,348 Views
LyncLin
Contributor III

用公司邮箱注册的账号开了一个新的问题,我将关闭这个问题,请在新的ticket下提供支持,感谢!

View solution in original post

0 Kudos
Reply
9 Replies
1,408 Views
guoweisun
NXP TechSupport
NXP TechSupport

VPRE/VCORE都是正常的吗?只有VAUX/VCCA有问题吗?

0 Kudos
Reply
1,396 Views
LyncLin
Contributor III

你好!

VPRE测得大约6.4V, VCORE1.25V, VCCA 3.28V. VAUX的三极管看起来处于截止状态,B级E级电压见问题描述。 VAUX和VCCA是同款三极管。外部电源输入12V,试过上升到18V,VAUX仍不工作。

0 Kudos
Reply
1,391 Views
guoweisun
NXP TechSupport
NXP TechSupport

你是学生?这个是学校的项目?还是什么?

0 Kudos
Reply
1,386 Views
LyncLin
Contributor III
Spoiler
我们是家方案公司,一个客户的项目
0 Kudos
Reply
1,380 Views
guoweisun
NXP TechSupport
NXP TechSupport

方便告知什么公司吗?以后提问题尽量用公司的邮箱,这样优先级很高,用自己的邮箱我们认为是C 客户就是可以支持但是如果我们很忙就会忽略掉C客户的问题。

0 Kudos
Reply
1,375 Views
LyncLin
Contributor III

论坛上不太方便,麻烦留个邮箱,稍后给您发个邮件吧。

0 Kudos
Reply
1,372 Views
guoweisun
NXP TechSupport
NXP TechSupport

Home (nxp.com)

用公司的邮箱上面的链接提问题,我们会回复的,私人、公司的问题不会被public post。 

0 Kudos
Reply
1,349 Views
LyncLin
Contributor III

用公司邮箱注册的账号开了一个新的问题,我将关闭这个问题,请在新的ticket下提供支持,感谢!

0 Kudos
Reply
1,387 Views
LyncLin
Contributor III
Spoiler
我们是企业,这是一个客户的项目。
0 Kudos
Reply