FS26 TRK2_UV

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS26 TRK2_UV

3,136 Views
dingyazhou
Contributor I

Hello, my FS26 will report TRK2_UV failure at the INIT_FS stage of the chip, so it cannot exit the INIT_FS stage, and the functional safety state machine is stuck. May I ask what is the cause

0 Kudos
Reply
15 Replies

503 Views
Vendrick
Contributor I

hi how can i use the VCORE to supply the VDD_LV of the MCP5746C

 

0 Kudos
Reply

3,122 Views
guoweisun
NXP TechSupport
NXP TechSupport

So for your FS26 setting TRK2_V_OTP [1:0] = 11 as 5.5V and actually it only has 5V,so it trigger UV threshold,right?

0 Kudos
Reply

1,532 Views
459021854
Contributor III
  • Hi, have you got the SCH-47651 schematics, if you have, can you share with me. Thanks
0 Kudos
Reply

1,537 Views
459021854
Contributor III

Hi, have you got the SCH-47651 schematics, if you have, can you share with me. Thanks

0 Kudos
Reply

3,116 Views
dingyazhou
Contributor I

It may be so, but the agent did not provide the documents for OTP configuration when buying the board. The model of FS26 is FS26AMDA0A1, and the model of development board is SCH-47651 REV A1

0 Kudos
Reply

3,112 Views
guoweisun
NXP TechSupport
NXP TechSupport

Understand, so you can  test the voltage of VTRK2 to confirm this voltage level and tell me the result.

0 Kudos
Reply

3,125 Views
guoweisun
NXP TechSupport
NXP TechSupport

what's the value of TRK2 in your board now? do you test it?

0 Kudos
Reply

3,123 Views
dingyazhou
Contributor I

As explained below, TRK2 and TRK1 are both 5V, now TRK2 will have an undervoltage flag to read the FS_OVUV_REG_STATUS register through SPI

0 Kudos
Reply

3,118 Views
guoweisun
NXP TechSupport
NXP TechSupport

Could you please share with your schematic?

0 Kudos
Reply

3,110 Views
dingyazhou
Contributor I

dingyazhou_0-1633759518620.jpeg

 

0 Kudos
Reply

3,088 Views
guoweisun
NXP TechSupport
NXP TechSupport

During the initialization phase, you can try to set VMON_TRK2_UV_FS_REACTION [1:0 ] as 00 to disable safety output and RSTB based on register of FS_I_OVUV_SAFE_REACTION2.

Use this method to eliminate the TRK2 UV affect.

0 Kudos
Reply

3,100 Views
guoweisun
NXP TechSupport
NXP TechSupport

Can you share the circuit of SCH-47651?

0 Kudos
Reply

3,092 Views
dingyazhou
Contributor I

Can you add a wechat for easy communication: 18196548686

dingyazhou_0-1633760502504.jpeg

 

0 Kudos
Reply

3,133 Views
guoweisun
NXP TechSupport
NXP TechSupport

Please measure the actual value of TRK2 and check whether the short circuit happened or not?

0 Kudos
Reply

3,130 Views
dingyazhou
Contributor I

The voltage of TRK2 and TRK1 is 5V, and now it is TRK2 undervoltage fault stuck functional safety state machine. The chip manual has such a sentence:  If the regulator is used as a global pin, outside of the module, it is recommended to not include it in power up sequence and turn on the regulator by SPI, to avoid a stuck in reset condition in case of short circuit.

0 Kudos
Reply