FS26 1.0.0 2209 installation issue within S32DS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS26 1.0.0 2209 installation issue within S32DS

1,482 Views
binli
NXP Employee
NXP Employee

Hi:

I just tried the latest FS26 driver package, FS26 1.0.0 D2209 installation in S32DS3.4. But it seems that there is problem with this installation package. Please see below for more detail:

'An error occurred while collecting items to be installed session context was:(profile=DefaultProfile, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).
Problems downloading artifact: binary, com.nxp.SBC_FS26.S32K3.1.0.0.win32.win32.x86_64,1.0.0.202209221325.
SHA-256 hash is not as expected. Expected: 66b59e489102f3976222b875625155e7e9c09f3ceb8eb0ad099506708b9ea4de and found a0941b275452889e84130cc9d7e0f1929dd9bd678eec1ebdeb05b7e286ba7c39.'

binli_1-1664247680848.png

Thanks.

0 Kudos
Reply
4 Replies

1,416 Views
cuongnguyenphu
NXP Employee
NXP Employee

Hi @binli ,
Sorry for this inconvenience, currently the package FS26 1.0.0 2209 is not able to install because of the bug in the release package. We're working on it to solve the problem.
You can try older version of FS26 as FS26 1.0.0 2208 CD01 or 0.9.1 instead:

cuongnguyenphu_0-1665391556521.png

cuongnguyenphu_1-1665391598124.png

 

 

1,411 Views
binli
NXP Employee
NXP Employee

Hi:

Got it, thanks.

0 Kudos
Reply

1,390 Views
cuongnguyenphu
NXP Employee
NXP Employee

The new release package for FS26 on S32K3XX is available on NXP product list, please take it for your note:

cuongnguyenphu_0-1665567627897.png

0 Kudos
Reply

1,384 Views
binli
NXP Employee
NXP Employee

Hi:

Well noted it, thanks.

0 Kudos
Reply