About MC33771C chipes first can't wakeup the seconed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

About MC33771C chipes first can't wakeup the seconed

1,958 次查看
Wan
Contributor II

Hi NXP sir,

       Recently, I am using MC33771, the battery management chip of your company. The environment I use is that S32K116 connects MC33664 through SPI,MC33664 connects MC33771 through TPL, and MC33771 connects to each other through capacitor.

The problem I encountered was:

         1. The first MC33771 can be woken up through the wake up sequence, but the second MC33771 does not respond. The wake up waveform of THE TPL signal line can not be collected from the first output signal line through oscilloscope. Perhaps this is the root cause of the failure to wake up. But I don't know why.

          2. In this environment, the LPSPI is configured as SLAVE mode and the data received is 6 bytes. However, in S32K116, the data can be configured as multiple of 4 bytes.

          3. Call LPSPI_DRV_SlaveTransfer() as SLAVE as LPSPI; Received, when I need to transfer 22 register information received message back error. Cannot read too much register information consecutively.

 

           The above are the problems I encountered when using your company's products, please answer them carefully! thank you

1.PNG2.PNG

0 项奖励
回复
5 回复数

1,884 次查看
Wan
Contributor II

OH,sorry.

    I found my problem,The first chip in my Daisy chain didn't init , but the first chip can be wakeup and go to IDE mode。

0 项奖励
回复

1,878 次查看
guoweisun
NXP TechSupport
NXP TechSupport

So you can wake up the followed BCC successfully ,right?

 

0 项奖励
回复

1,929 次查看
guoweisun
NXP TechSupport
NXP TechSupport

In your system, except wake up function fail, does have any other issue?

0 项奖励
回复

1,943 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Is possible to share with your schematic here?

 

0 项奖励
回复

1,940 次查看
Wan
Contributor II

 

 

3.PNG

This is the first piece of MC33771. The front is connected to the MC33664 by transformer, and the back is connected to the MC33771 by capacitor  

this is my wake up timing:

PINS_DRV_WritePin(PCS_USER_PORT, PCS_USER_PIN, 0u);     //down

BCC_WaitUs(20U);

PINS_DRV_WritePin(PCS_USER_PORT, PCS_USER_PIN, 1u);    //up

BCC_WaitUs(510U);

PINS_DRV_WritePin(PCS_USER_PORT, PCS_USER_PIN, 0u);   //down

BCC_WaitUs(20U);

PINS_DRV_WritePin(PCS_USER_PORT, PCS_USER_PIN, 1u);   //up

 

0 项奖励
回复