dear all
I am trying to erase the nor flash in the elbc bus of the p2041 for programming the boot code it is providing me sector protection error can this be because of this pins are not proper
the
1. TMP_DETECT
2.LP_TMP_DETECT
3.PO_VDD
in AN4402 pg33
It is mentioned that
TMP_DETECT -----Tie high to OVDD (high-power Trust
Architecture is not used).
LP_TMP_DETECT------Tie high to VDD_LP (low-power Trust
Architecture is not used).
If no aspect of Trust Architecture is
used, the following Trust Architecture
pins can be tied to GND:
– PO_VDD
– TMP_DETECT
– LP_TMP_DETECT
if i dont need any trust feature feature i have to tie the pins to GND ?