Hello,
I progrmmed NOR Flash with NOR Flash Image came with P2041RDB board. Board is booting fine but ethernet Interfaces are not working...(attached the screen shot) Please assist me.
Thanks & Regards,
Veerendranath Jakkam
Hello veerendranath jakkam,
Please also update FMAN microcode, which should be compatible with u-boot image, you could get it from Linux SDK pre-built image ISO.
In addition, would you please provide the whole u-boot log? I want to check u-boot version information.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks for the reply,
where to get the updated " Linux SDK pre-built image ISO". Please provide the link. please check following images for uboot log.
Hello veerendranath jakkam,
Please download SDK 1.8 image ISO for E500MC platform from Linux® SDK for QorIQ Processors v1.8|Freescale, then program u-boot, ucode for CPU 2.0, and RCW for 5G.
Then under u-boot prompt, please provide the result of command "mii info" to get PHY info.
> mii info
PHY 0x00: OUI = 0x01C1, Model = 0x03, Rev = 0x01, 10baseT, HDX
PHY 0x01: OUI = 0x01C1, Model = 0x03, Rev = 0x01, 10baseT, HDX
PHY 0x02: OUI = 0x03F1, Model = 0x15, Rev = 0x01, 10baseT, HDX
PHY 0x03: OUI = 0x03F1, Model = 0x15, Rev = 0x01, 10baseT, HDX
PHY 0x04: OUI = 0x03F1, Model = 0x15, Rev = 0x01, 10baseT, HDX
PHY 0x1F: OUI = 0x0000, Model = 0x00, Rev = 0x00, 1000baseX, HDX
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
current NOR flash binary i am using is "QorIQ_SDK_V1.4_P2041RDB_20130625_NOR_Flash.bin"... but when I boot the device with that binary file Ethernet ports are not working... where can I get latest version (i.e. SDK_V1.8) of NOR flash binary image?. In the link provided by you only ISO images are there...no NOR flash binary images available...
Thanks and Regards,
Veerendranath
Hello veerendranath jakkam,
You could download the ISO "QorIQ SDK v1.8 PPCE500MC IMAGE yocto" from the above link, which contains the prebuilt image ISO.
Previously I suspect whether this problem is related with CPLD, because the CPLD version is 4.0 on our board farm boards, but on your target is CPLD 4.1. I verified SDK 1.4 u-boot on my P2040 target board with CPLD 4.1 without problem, I suggest you do the following.
Under u-boot, please use "mii info" command to check PHY information, if the result is abnormal, probably there is quality problem, please submit a service request in our CRM system to require further assistance.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hello Yiping,
I have updated the flash with latest image(SDK1.8) as you instructed but still issue is not resolved. Please find the screen shots. you can find "mii info" command information also.
Regards,
Veerendrnath
Hello veerendranath jakkam,
According to the u-boot log, it looks that this is not a software problem, there should be hardware problem on this target board, please submit a service request in our internal CRM system for further assistance.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Please provide information regarding your Internal CRM system weblink and details I need to submit to raise a request...
Thanks and Regards,
Veerendranath