Whenever I run bitbake, I get these warning messages. How do I fix this?
$ bitbake -c cleansstate virtual/kernel
WARNING: Duplicate inclusion for /home/timur/QorIQ-SDK-V1.9-20151210-yocto/sources/meta-freescale-internal/conf/distro/imagedepends.conf in /home/timur/QorIQ-SDK-V1.9-20151210-yocto/sources/meta-freescale-internal/conf/layer.conf
WARNING: Duplicate inclusion for /home/timur/QorIQ-SDK-V1.9-20151210-yocto/sources/meta-freescale-internal/conf/distro/url-sha-references.conf in /home/timur/QorIQ-SDK-V1.9-20151210-yocto/sources/meta-freescale-internal/conf/layer.conf
WARNING: Duplicate inclusion for /home/timur/QorIQ-SDK-V1.9-20151210-yocto/sources/meta-virtualization/conf/distro/include/virt_security_flags.inc in /home/timur/QorIQ-SDK-V1.9-20151210-yocto/sources/meta-virtualization/conf/layer.conf
Loading cache: 100% |###########################################| ETA: 00:00:00
Loaded 3251 entries from dependency cache.
WARNING: No bb files matched BBFILE_PATTERN_openembedded-layer '^/home/timur/QorIQ-SDK-V1.9-20151210-yocto/sources/meta-openembedded/meta-oe/'
WARNING: No bb files matched BBFILE_PATTERN_multimedia-layer '^/home/timur/QorIQ-SDK-V1.9-20151210-yocto/sources/meta-openembedded/meta-multimedia/'
WARNING: No bb files matched BBFILE_PATTERN_networking-layer '^/home/timur/QorIQ-SDK-V1.9-20151210-yocto/sources/meta-openembedded/meta-networking/'
WARNING: No bb files matched BBFILE_PATTERN_perl-layer '^/home/timur/QorIQ-SDK-V1.9-20151210-yocto/sources/meta-openembedded/meta-perl/'
WARNING: No bb files matched BBFILE_PATTERN_meta-python '^/home/timur/QorIQ-SDK-V1.9-20151210-yocto/sources/meta-openembedded/meta-python/'
WARNING: No bb files matched BBFILE_PATTERN_ruby-layer '^/home/timur/QorIQ-SDK-V1.9-20151210-yocto/sources/meta-openembedded/meta-ruby/'
WARNING: No bb files matched BBFILE_PATTERN_filesystems-layer '^/home/timur/QorIQ-SDK-V1.9-20151210-yocto/sources/meta-openembedded/meta-filesystems/'
WARNING: No bb files matched BBFILE_PATTERN_webserver '^/home/timur/QorIQ-SDK-V1.9-20151210-yocto/sources/meta-openembedded/meta-webserver/'
WARNING: No bb files matched BBFILE_PATTERN_toolchain-layer '^/home/timur/QorIQ-SDK-V1.9-20151210-yocto/sources/meta-openembedded/toolchain-layer/'
NOTE: Resolving any missing task queue dependencies
The duplicate inclusion warnings are caused by sourcing fsl-setup-env on an existing build. A side effect of this is that layer.conf and bblayers.conf get duplicate lines appended. You can simply remove the duplicate lines and the warnings will go away.
Hi,
It means your .conf files are including some other conf/inc files mutiple times. Like in your case layer.conf is including imagedepends.conf, url-sha-references.conf and virt_security_flags.inc files multiple times.
How do I fix it? I didn't edit layer.conf. I just did a normal SDK installation following the directions. Here's my layer.conf:
# We have a packages directory, add to BBFILES
BBPATH .= ":${LAYERDIR}"
BBFILES += "${LAYERDIR}/recipes-*/*/*.bb"
BBFILES += "${LAYERDIR}/recipes-*/*/*.bbappend"
BBFILES += "${LAYERDIR}/classes/*.bb"
BBFILE_COLLECTIONS += "fsl-internal"
BBFILE_PATTERN_fsl-internal = "^${LAYERDIR}/"
BBFILE_PRIORITY_fsl-internal = "5"
LICENSE_PATH += "${LAYERDIR}/licenses"
# Let us add layer-specific bbappends which are only applied when that
# layer is included in our configuration
BBFILES += "${@' '.join('${LAYERDIR}/dynamic-layers/%s/recipes*/*/*.bbappend' % layer \
for layer in BBFILE_COLLECTIONS.split())}"
BBFILES += "${@' '.join('${LAYERDIR}/dynamic-layers/%s/recipes*/*/*.bb' % layer \
for layer in BBFILE_COLLECTIONS.split())}"
include conf/distro/imagedepends.conf
include conf/distro/url-sha-references.conf
and here's my imagedepends.conf:
# pkgs to be installed for specific board
EXTRA_IMAGEDEPENDS_append_p1020rdb = " vsc7385-firmware"
EXTRA_IMAGEDEPENDS_append_p1021rdb = " vsc7385-firmware"
EXTRA_IMAGEDEPENDS_append_p1022ds = " edink"
EXTRA_IMAGEDEPENDS_append_p2020rdb = " vsc7385-firmware"
EXTRA_IMAGEDEPENDS_append_t2080rdb = " cs4315-firmware"
EXTRA_IMAGEDEPENDS_append_t2080rdb-64b = " cs4315-firmware"
EXTRA_IMAGEDEPENDS_append_t4240rdb = " cs4315-firmware"
EXTRA_IMAGEDEPENDS_append_t4240rdb-64b = " cs4315-firmware"
I don't see any duplicates anywhere.
Hello Timur Tabi,
The problem should exist in your procedure to create the build project, please refer to my attached local.conf in build_p1022ds/conf/, I think it should be different with yours.
Please remove the folder "build_p1022ds", go to the folder <install folder>/QorIQ-SDK-V1.9-20151210-yocto, and execute the command "source ./fsl-setup-env -m p1022ds"(please note that you need to finishing reading the EULA information and accept it) , then run bitbake command.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------