Hello,
I ve got a P1021rdb-PC board and I have to configure so that it boots from the EEPROM SPI Flash.
I want to write the SPI bootloader to the corresponding
Here is what I do:
cat /pro/ c/mtd
dev: size erasesize name
mtd0: 00040000 00020000 "NOR Vitesse-7385 Firmware"
mtd1: 00040000 00020000 "NOR DTB Image"
mtd2: 00380000 00020000 "NOR Linux Kernel Image"
mtd3: 00b00000 00020000 "NOR JFFS2 Root File System"
mtd4: 00100000 00020000 "NOR U-Boot Image"
mtd5: 00100000 00004000 "NAND U-Boot Image"
mtd6: 00100000 00004000 "NAND DTB Image"
mtd7: 00400000 00004000 "NAND Linux Kernel Image"
mtd8: 00400000 00004000 "NAND Compressed RFS Image"
mtd9: 00700000 00004000 "NAND JFFS2 Root File System"
mtd10: 00f00000 00004000 "NAND Writable User area"
mtd11: 000a0000 00010000 "SPI Flash U-Boot Image"
mtd12: 00060000 00010000 "SPI Flash DTB Image"
mtd13: 00400000 00010000 "SPI Flash Linux Kernel Image"
mtd14: 00400000 00010000 "SPI Flash Compressed RFSImage"
mtd15: 00700000 00010000 "SPI Flash JFFS2 RFS"
root@p1021rdb:~# ls /dev/mtd*s -l
crw------- 1 root root 90, 0 Jan 1 1970 /dev/mtd0
crw------- 1 root root 90, 1 Jan 1 1970 /dev/mtd0ro
crw------- 1 root root 90, 2 Jan 1 1970 /dev/mtd1
crw------- 1 root root 90, 20 Jan 1 1970 /dev/mtd10
crw------- 1 root root 90, 21 Jan 1 1970 /dev/mtd10ro
crw------- 1 root root 90, 22 Jan 1 1970 /dev/mtd11
crw------- 1 root root 90, 23 Jan 1 1970 /dev/mtd11ro
crw------- 1 root root 90, 24 Jan 1 1970 /dev/mtd12
crw------- 1 root root 90, 25 Jan 1 1970 /dev/mtd12ro
crw------- 1 root root 90, 26 Jan 1 1970 /dev/mtd13
crw------- 1 root root 90, 27 Jan 1 1970 /dev/mtd13ro
crw------- 1 root root 90, 28 Jan 1 1970 /dev/mtd14
crw------- 1 root root 90, 29 Jan 1 1970 /dev/mtd14ro
crw------- 1 root root 90, 30 Jan 1 1970 /dev/mtd15
crw------- 1 root root 90, 31 Jan 1 1970 /dev/mtd15ro
crw------- 1 root root 90, 3 Jan 1 1970 /dev/mtd1ro
crw------- 1 root root 90, 4 Jan 1 1970 /dev/mtd2
crw------- 1 root root 90, 5 Jan 1 1970 /dev/mtd2ro
crw------- 1 root root 90, 6 Jan 1 1970 /dev/mtd3
crw------- 1 root root 90, 7 Jan 1 1970 /dev/mtd3ro
crw------- 1 root root 90, 8 Jan 1 1970 /dev/mtd4
crw------- 1 root root 90, 9 Jan 1 1970 /dev/mtd4ro
crw------- 1 root root 90, 10 Jan 1 1970 /dev/mtd5
crw------- 1 root root 90, 11 Jan 1 1970 /dev/mtd5ro
crw------- 1 root root 90, 12 Jan 1 1970 /dev/mtd6
crw------- 1 root root 90, 13 Jan 1 1970 /dev/mtd6ro
ct 90, 14 Jan 1 1970 /dev/mtd7
crw------- 1 root root 90, 15 Jan 1 1970 /dev/mtd7ro
crw------- 1 root root 90, 16 Jan 1 1970 /dev/mtd8
crw------- 1 root root 90, 17 Jan 1 1970 /dev/mtd8ro
crw------- 1 root root 90, 18 Jan 1 1970 /dev/mtd9
crw------- 1 root root 90, 19 Jan 1 1970 /dev/mtd9ro
brw-rw---- 1 root disk 31, 0 Jan 1 1970 /dev/mtdblock0
brw-rw---- 1 root disk 31, 1 Jan 1 1970 /dev/mtdblock1
brw-rw---- 1 root disk 31, 10 Jan 1 1970 /dev/mtdblock10
brw-rw---- 1 root disk 31, 11 Jan 1 1970 /dev/mtdblock11
brw-rw---- 1 root disk 31, 12 Jan 1 1970 /dev/mtdblock12
brw-rw---- 1 root disk 31, 13 Jan 1 1970 /dev/mtdblock13
brw-rw---- 1 root disk 31, 14 Jan 1 1970 /dev/mtdblock14
brw-rw---- 1 root disk 31, 15 Jan 1 1970 /dev/mtdblock15
brw-rw---- 1 root disk 31, 2 Jan 1 1970 /dev/mtdblock2
brw-rw---- 1 root disk 31, 3 Jan 1 1970 /dev/mtdblock3
brw-rw---- 1 root disk 31, 4 Jan 1 1970 /dev/mtdblock4
brw-rw---- 1 root disk 31, 5 Jan 1 1970 /dev/mtdblock5
brw-rw---- 1 root disk 31, 6 Jan 1 1970 /dev/mtdblock6
brw-rw---- 1 root disk 31, 7 Jan 1 1970 /dev/mtdblock7
brw-rw---- 1 root disk 31, 8 Jan 1 1970 /dev/mtdblock8
brw-rw---- 1 root disk 31, 9 Jan 1 1970 /dev/mtdblock9
root@p1021rdb:~# flash_eraseall /dev/mtd11
flash_eraseall has been replaced by `flash_erase <mtddev> 0 0`; please use it
flash_erase: error!: /dev/mtd11
error 13 (Permission denied)
These Character devices (mtdxx) have even minor number. They seem to be OK. What I m missing here??
even "cat /dev/null > /dev/mtd11" doesnt work
Please Help!!
Thank you very much in advance!!
已解决! 转到解答。
Hi Scott,
thanks for the reply!!. You ve pointed out exactly what i was missing! Now I am able to run U-Boot from SPI flash. However, I have some problems as U-boot runs the ramdisk image that has been successfully tftped at an address. At one point, the system hangs. Here is the log
U-Boot 2011.12-00064-gbfb0c9a (Nov 15 2012 - 23:28:50)
CPU0: P1021E, Version: 1.1, (0x80ec0111)
Core: E500, Version: 5.1, (0x80212051)
Clock Configuration:
CPU0:800 MHz, CPU1:800 MHz,
CCB:400 MHz,
DDR:333.333 MHz (666.667 MT/s data rate) (Asynchronous), LBC:25 MHz
QE:400 MHz
L1: D-cache 32 kB enabled
I-cache 32 kB enabled
Board: P1021RDB CPLD: V4.1 PCBA: V4.0
Error reading i2c boot information!
I2C: ready
SPI: ready
DRAM: DDR: failed to read SPD from address 82 :smileyalert:
Error in DDR bus width configuration! :smileyalert:
16 MiB (DDR3, 32-bit, CL=6, ECC off)
Flash: 16 MiB
L2: 256 KB enabled
NAND: 32 MiB
MMC: FSL_SDHC: 0
SF: Detected S25FL128P_64K with page size 64 KiB, total 16 MiB
Firmware 'Microcode version 0.0.1 for P1021 r1.0' for 1021 V1.0
QE: uploading microcode 'Microcode for P1021 r1.0' version 0.0.1
PCIe1: Root Complex of mini PCIe SLOT, no link, regs @ 0xffe0a000
PCIe1: Bus 00 - 00
PCIe2: Endpoint of PCIe SLOT, no link, regs @ 0xffe09000
PCIe2: Bus 01 - 01
In: serial
Out: serial
Err: serial
Net: eTSEC2 is in sgmii mode.
uploading VSC7385 microcode from ef020000
PHY reset timed out
eTSEC1, eTSEC2, eTSEC3
Hit any key to stop autoboot: 10 0
=> run ramboot
Speed: 1000, full duplex
Using eTSEC1 device
TFTP from server 10.a.b.c; our IP address is 10.d.e.f
Filename 'rootfs.ext2.gz.u-boot'.
Load address: 0x2000000
Loading: *#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#######################
done
Bytes transferred = 28954008 (1b9cd98 hex)
Speed: 1000, full duplex
Using eTSEC1 device
TFTP from server 10.a.b.c; our IP address is 10.d.e.f
Filename 'uImage-p1021rdb.bin'.
Load address: 0x1000000
Loading: *#################################################################
#################################################################
#################################################################
####################################################
done
Bytes transferred = 3620878 (37400e hex)
Speed: 1000, full duplex
Using eTSEC1 device
TFTP from server 10.a.b.c; our IP address is 10.d.e.f
Filename 'uImage-p1021rdb.dtb'.
Load address: 0xc00000
Loading: *##
done
Bytes transferred = 25245 (629d hex)
## Booting kernel from Legacy Image at 01000000 ...
Image Name: Linux-3.0.34-rt55-02404-g1a39570
Created: 2012-11-30 13:55:59 UTC
Image Type: PowerPC Linux Kernel Image (gzip compressed)
Data Size: 3620814 Bytes = 3.5 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
## Loading init Ramdisk from Legacy Image at 02000000 ...
Image Name: fsl-image-core-p1021rdb-20121116
Created: 2012-11-16 9:09:58 UTC
Image Type: PowerPC Linux RAMDisk Image (gzip compressed)
Data Size: 28953944 Bytes = 27.6 MiB :smileyalert:
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
## Flattened Device Tree blob at 00c00000
Booting using the fdt blob at 0x00c00000
Uncompressing Kernel Image ... OK
ERROR: Failed to allocate 0x1b9cd58 bytes below 0xffffffff.
ramdisk - allocation error :smileyalert:
Then, the system hangs here
It seems like I can't load the 27MB Ramdisk file using SPI-Uboot. Is it due to the DDR Configuration in the Uboot.bin file? Wrong DDR Bus Width configuration??
What should I do to fix this?
Please Help
Thank you very much
You seem to have a problem with the DDR configuration:
DRAM: DDR: failed to read SPD from address 82 :smileyalert:
Error in DDR bus width configuration! :smileyalert:
16 MiB (DDR3, 32-bit, CL=6, ECC off)
This is a separate problem that should be posted under its own title, so that the relevant people will see it.