I am running kernel
Linux freescale 2.6.32-svn1457 #178 SMP Thu Jul 7 10:40:12 EDT 2011 ppc unknown
If I send 10,000 16k packets over TCP, the P2020 will receive most of them in about 1.5 microseconds. However,
about 500 times in this test, not all characters are received and it takes about 300 milliseconds for the
packet to come in.
Probably what's happening is that the linux tcp stack is timing out at 200 ms before continuing to receive the
packet stream.
I can ameliorate the problem by sending back a \0 byte ever time I receive a partial packet. Then all runs well,
as the stack is piggy-backing the ACK/NAK on this packet.
But, is there either:
1. A patch to the linux kernel to resolve this issue?
2. Or, is that a network parameter I can change to do same?
Thank You,
Cal Page
Teradyne