UCC UART Speed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UCC UART Speed

842件の閲覧回数
naveennaga
Contributor I

Hi All,

We are using p1021 processor in our project. Quick engine UCC will be used as UART in synchronous mode. We want to achieve 2 Mbps  with UCC configured in slow protocol and UART in NSMI mode.

Can we achieve with slow protocol UCC UART? If so can you guide to the register configuration for clock setting and other.

ラベル(1)
タグ(3)
0 件の賞賛
3 返答(返信)

634件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at the Section 17.1, 17.1.3.2 and Table 17-6 of the QUICC Engine Block Reference Manual (https://www.freescale.com/webapp/Download?colCode=QEIWRM&location=null&fpsp=1&WT_TYPE=Reference%20Ma...).

The P1021 UCC UART supports 2 Mbps with UCC configured in slow protocol and UART in NSMI mode.

Freescale offers CPM performance calculator for the MPC82xx (http://www.freescale.com/webapp/sps/download/license.jsp?colCode=MPC8260CALC2&location=null&Parent_n...).

This calculator can be used as lower estimation UCC UART.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

634件の閲覧回数
naveennaga
Contributor I

Thank You Pavel.

I'm referring the ucc_uart.c low driver code from QorIQ 1.7 SDK to

implement the synchronous UART with enabling RTS,CTS,CD and DTR , DSR ,RI

as gpios .

Is there any sample device tree for enabling these control signals and code

for control of this signals during Tx and Rx.

0 件の賞賛

634件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at the following page:

http://www.freescale.com/infocenter/index.jsp?topic=%2FQORIQSDK%2F2151457.html

This driver can be used as example using additional signals of the RS-232.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛