TDM on P1020 within vxWorks

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TDM on P1020 within vxWorks

1,193 Views
naumgrutman
Contributor II

To anybody that has experience with P1020 and TDM,

I have a question a question about TDM on P1020

I have the TDM working just fine on within Linux and trying to make it it work within vxWorks

I have put together the the TDM driver for vxWorks based on the Linux driver within your SDK and also based on P1020 QorIQ Reference Manual Rev.6 page# 1519

I do steps 1 thru 4 and based on item number 5 I have to read the TSR and RSR and wait for those to get on...

but they never do... Could you shed some light on this subject...

  1. Bring the chip out of reset.
  2. Program the TDM control registers-TDM RIR, TDM RFP, TDM TIR, TDM TFP,

and TDM GIR.

  1. Program all channel enable registers (TDM RCENn , TDM TCENn ) and transmit

channel mask registers (TDM TCMAn ) as disabled.

  1. Enable the TDM Rx and Tx by setting the TDM RCR[REN] and TDM TCR[TEN]

bits.

  1. Wait until TDM TSR[TENS] and TDM RSR[RENS] are set.
  2. If the TDM is serviced by:
  3. DMA transfer-immediately use a software started DMA channel to write data to

the Tx data register(s) (must be completed before two Tx frame syncs arrive

after enabling).

  1. Interrupts-immediately write data to the Tx data register(s) (must be completed

before two Tx frame syncs arrive after enabling).

  1. Follow the steps outlined in Dynamic channel configuration while TDM operating-shared,

to enable channels.

  1. All other writes and reads will be initiated by either an interrupt or a DMA request,

depending on the configuration.

On Linux TDM TSR and TDM RSR  do get set

====================================

F519A000: 00000001 0000E241 0000E041 007F0030  .......A...A...0

F519A010: 007F0030 007F0030 007F0030 007F0030  ...0...0...0...0

F519A020: FFFFFFFF FFFFFFFF FFFFFFFF FFFFFFFF  ................

F519A030: FFFFFFFF FFFFFFFF FFFFFFFF FFFFFFFF  ................

F519A040: FFFFFFFF FFFFFFFF FFFFFFFF FFFFFFFF  ................

F519A050: FFFFFFFF FFFFFFFF FFFFFFFF FFFFFFFF  ................

F519A060: 00000000 00000000 00000000 00000000  ................

F519A070: 00000000 00000000 00000000 00000000  ................

F519A080: 00000001 00000001 00000000 00000000  ................

F519A090: 00000000 00000000 00000000 00000000  ................

F519A0A0: 000001C0 000001C0 00000005 00000025  ...............%

On vxWorks instead of TSR and RSR I get 0x00000001 in Reserved fields marked in RED

==========================================================================

F3016000: 00000001 0000E241 0000E041 007F0030  .......A...A...0

F3016010: 007F0030 007F0030 007F0030 007F0030  ...0...0...0...0

F3016020: FFFFFFFF FFFFFFFF FFFFFFFF FFFFFFFF  ................

F3016030: FFFFFFFF FFFFFFFF FFFFFFFF FFFFFFFF  ................

F3016040: FFFFFFFF FFFFFFFF FFFFFFFF FFFFFFFF  ................

F3016050: FFFFFFFF FFFFFFFF FFFFFFFF FFFFFFFF  ................

F3016060: 00000000 00000000 00000000 00000000  ................

F3016070: 00000000 00000000 00000000 00000000  ................

F3016080: 00000001 00000001 00000000 00000000  ................

F3016090: 00000001 00000001 00000001 00000001  ................

F30160A0: 00000000 00000000 00000000 00000000  ................

 

Could you shed some light on this subject...

Thanks,

Naum

Labels (1)
0 Kudos
Reply
3 Replies

969 Views
Pavel
NXP Employee
NXP Employee

We do not have experience for VxWork using.

It looks like that debugging of your VxWorks driver is needed.

Have a great day,
Pavel Chubakov

0 Kudos
Reply

969 Views
Pavel
NXP Employee
NXP Employee

Documentation for the P1020 does not have information about these reserved register.

Do you see incorrect behavior for your driver for the P1020 TDM?

Have a great day,
Pavel Chubakov

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

969 Views
naumgrutman
Contributor II

Hello Pavel,

 

Let me clarify…

Within Linux environment P1020 TDM Regs at offset 0x16000 from CCSR

are mapped by Linux 0xFFE016000 -> 0xF519A000

Within Linux environment I do not have issues with TDM driver

as far as what I need the TDM driver to perform…



On Linux TDM TSR and TDM RSR  do get set

====================================

F519A000: 00000001 0000E241 0000E041 007F0030  .......A...A...0

F519A010: 007F0030 007F0030 007F0030 007F0030  ...0...0...0...0

F519A020: FFFFFFFF FFFFFFFF FFFFFFFF FFFFFFFF  ................

F519A030: FFFFFFFF FFFFFFFF FFFFFFFF FFFFFFFF  ................

F519A040: FFFFFFFF FFFFFFFF FFFFFFFF FFFFFFFF  ................

F519A050: FFFFFFFF FFFFFFFF FFFFFFFF FFFFFFFF  ................

F519A060: 00000000 00000000 00000000 00000000  ................

F519A070: 00000000 00000000 00000000 00000000  ................

F519A080: 00000001 00000001 00000000 00000000  ................

F519A090: 00000000 00000000 00000000 00000000  ................

F519A0A0: 000001C0 000001C0 00000005 00000025  ...............%

 

When TCR gets set @ 0xF519A084 to 0x00000001 within microseconds

0xF519A0AC gets set in response to 0x00000025

and

0xF519A0A4 get set to 0x000001C0

 

When RCR gets set @ 0xF519A080 to 0x00000001 within microseconds

0xF519A0A8 gets set in response to 0x00000005

and

0xF519A0A0 get set to 0x000001C0

 

above line marked in green @ 0xF519A0A0 shows good results

Especially the fact that ReadOnly registers TDM TSR[TENS] and TDM RSR[RENS]

are set since this is what is needed for Step #5 on P1020 QorIQ Reference

Manual Rev.6 Chapter 19 page # 1519

  

Within vxWorks environment P1020 TDM Regs at offset 0x16000 from CCSR

are at 0xF3016000

I have adopted the TDM driver from Linux and rebuilt it for VxWorks environment

to do/accomplish the same data structures and tasks as they appear and performed

within Linux environment… 97 to 98% of the work is done…

The last girdle is that when TCR and RCR get set similar to the steps described above…

instead getting ReadOnly registers TDM TSR[TENS] and TDM RSR[RENS] set

I see that Reserved Area @ 0xF3016090 gets set to 0x00000001 as marked in RED

which should be an indication of something… but there is no documentation

how this should deciphered…TSR and RSR never get set and I cannot force them

since these are Read-Only fields... P1020 processor is in control...

P1020 processor sets the reserved fields to 0x00000001 which is indication of something

but what nobody knows since there is no documentation on these reserved fields...

 

On vxWorks instead of TSR and RSR I get 0x00000001 in Reserved fields marked in RED

==========================================================================

F3016000: 00000001 0000E241 0000E041 007F0030  .......A...A...0

F3016010: 007F0030 007F0030 007F0030 007F0030  ...0...0...0...0

F3016020: FFFFFFFF FFFFFFFF FFFFFFFF FFFFFFFF  ................

F3016030: FFFFFFFF FFFFFFFF FFFFFFFF FFFFFFFF  ................

F3016040: FFFFFFFF FFFFFFFF FFFFFFFF FFFFFFFF  ................

F3016050: FFFFFFFF FFFFFFFF FFFFFFFF FFFFFFFF  ................

F3016060: 00000000 00000000 00000000 00000000  ................

F3016070: 00000000 00000000 00000000 00000000  ................

F3016080: 00000001 00000001 00000000 00000000  ................

F3016090: 00000001 00000001 00000001 00000001  ................

F30160A0: 00000000 00000000 00000000 00000000  ................

 

Could you provide additional info or shed some light on this subject...

Thanks,

Naum

 

0 Kudos
Reply