Hi All,
I am of the P2041RDB-PC EVM board test.
In the existing T2081 Board has set the boot as shown below.
=> tftp 1000000 u-boot-sd-T2080RDB_SDCARD.bin
=> write 1000000 8 0x800
=> 1000000 fsl_fman_ucode_T2080_xx.bin
=> write 1000000 0x820 80
P2041RDB-PC on the CD, download the u-boot-sd-P2041RDB SDCARD-git-r34.bin fsl_fman_ucode_p2041_r2.0_106_1_9.bin and below were not to boot.
=> tftp 1000000 u-boot-sd-P2041RDB_SDCARD-git-r34.bin
=> mmc write 1000000 0x008 0x800
=> tftp 1000000 fsl_fman_ucode_p2041_r2.0_106_1_9.bin
=> mmc write 1000000 0x46a 0x080
Did you write the wrong address? Or how all right the wrong?
Thank you.
Best regards,
gyosun.