Hello All -
I've been trying, without success, to build the toolchaing for QT Embedded with 1.4 QorIO SDK.
I am setup for a p1022ds and when I run "bitbake meta-toolchain-qte" it fails with:
ERROR: QA Issue: nativesdk-qemu rdepends on nativesdk-dtc-dev
ERROR: QA run found fatal errors. Please consider fixing them.
ERROR: Function failed: do_package_qa
ERROR: Logfile of failure stored in: /home/jcoffin/yocto-fsl/QorIQ-SDK-V1.4-20130625-yocto/build_p1022ds_release/tmp/work/x86_64-nativesdk-fsl_networking_sdk-linux/nativesdk-qemu/1.4.0-r0/temp/log.do_package.13118
ERROR: Task 850 (virtual:nativesdk:/home/jcoffin/yocto-fsl/QorIQ-SDK-V1.4-20130625-yocto/meta/recipes-devtools/qemu/qemu_1.4.0.bb, do_package) failed with exit code '1'
Anyone have any suggestions?
I'm not familiar with the QT Embedded toolchain, but my problem with the regular toolchain was that I was executing:
bitbake meta-toolchain
instead of:
bitbake fsl-toolchain
... for others benefit.
This one just popped up on me ... did you find the solution?