Hello,
I am trying to set up the DHCP ethernet connection of my p4080ds board. I am using the core image. I use a switch to connect host system and my board.
After boot up, the board alerts the following message:
WARNING: adjusting available memory to 30000000
Wrong Image Format for bootm command
ERROR: can't get kernel image!
So I use "pix altbank" to boot up in alternative bank. After I enter the system, I type ifconfig. But it seems there is no eth0 interface.
root@p4080ds:~# ifconfig -a
fm1-10g Link encap:Ethernet HWaddr 00:e0:0c:00:d7:04
BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Memory:fe4f0000-fe4f0fff
fm1-gb1 Link encap:Ethernet HWaddr 00:e0:0c:00:d7:01
BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Memory:fe4e2000-fe4e2fff
fm2-10g Link encap:Ethernet HWaddr 00:e0:0c:00:d7:09
BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Memory:fe5f0000-fe5f0fff
fm2-gb2 Link encap:Ethernet HWaddr 00:e0:0c:00:d7:07
BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Memory:fe5e4000-fe5e4fff
fm2-gb3 Link encap:Ethernet HWaddr 00:e0:0c:00:d7:08
BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Memory:fe5e6000-fe5e6fff
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:16436 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
sit0 Link encap:UNSPEC HWaddr 00-00-00-00-00-00-00-00-00-00-00-00-00-00-
NOARP MTU:1480 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
tunl0 Link encap:IPIP Tunnel HWaddr
NOARP MTU:1480 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
How can I solve this? Thanks, have a great day!
Regards,
Peter Zheng
解決済! 解決策の投稿を見る。
Hello Peter,
Please refer to "3.2.23.2.3.1.4 SerDes Protocol 0xe, P4080 Rev 2, Total Capacity 23 Gbps" in SDK document, please check whether the physical network connection is correct, then configure IP address for "fm*-gb*".
Thanks,
Yiping
Hello Peter,
On P4080DS Linux System, Ethernet ports on PCIe Network interface (XAUI) card are name as eth* interface.
Thanks,
Yiping
Hi Yiping,
Do you know how could I set up the internet to make P4080DS connect to internet?
Regards,
Peter
Hello Peter,
Please refer to "3.2.23.2.3.1.4 SerDes Protocol 0xe, P4080 Rev 2, Total Capacity 23 Gbps" in SDK document, please check whether the physical network connection is correct, then configure IP address for "fm*-gb*".
Thanks,
Yiping
Hello Peter,
On DPAA(including P4080DS) target board, we don't use eth* naming convention, we use fm*-gb* in Linux Kernel instead, which means the ethernet ports connecting to FMAN, please refer to the following port mapping for the RCW which you are use on this bank.
U-boot Port i Linux FMAN Address
FM1@DTSEC2 fm1-gb1 0xffe4e2000
FM1@TGEC1 fm1-10g 0xffe4f0000
FM2@DTSEC3 fm2-gb2 0xffe5e4000
FM2@DTSEC4 fm2-gb3 0xffe5e6000
FM2@TGEC1 fm2-10g 0xffe5f0000
You could get detailed information in p4080ds.dts,
fman0: fman@400000 {
... ...
enet1: ethernet@e2000 {
tbi-handle = <&tbi1>;
phy-handle = <&phy1>;
phy-connection-type = "sgmii";
};
... ...
enet4: ethernet@f0000 {
phy-handle = <&phy10>;
phy-connection-type = "xgmii";
};
}
fman1: fman@500000 { |
... ...
enet7: ethernet@e4000 {
tbi-handle = <&tbi7>;
phy-handle = <&phy7>;
phy-connection-type = "sgmii";
};
enet8:ethernet@e6000 { | |
tbi-handle = <&tbi8>; | |
phy-handle = <&phy8>; | |
phy-connection-type = "sgmii"; | |
}; |
enet9: ethernet@f0000 { | |
phy-handle = <&phy11>; | |
phy-connection-type = "xgmii"; | |
}; } |
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------