Dear sir
Could anyone provide me ngPIXIS A3P600-FGG484 fpga image of P4080DS board?
thanks!
best regards!
yanwang
I want to re-program the on board FPGA in P4080DS, because the board always works in hang status.
> works in hang status
What exactly does it mean?
What are states of all on-board LEDs when power is on?
The P4080DS does not switch to reset status when i press the reset button. But the power supply to board is good and LED is all on.
Please provide clear photo of all on-board LEDs.
Please attach separate +12V ATX connector - it is not connected in the provided picture.
Attached the board with ATX power supply.
It is required to use ATX2 power supply.
It must have 24-pin main connector and dedicated +12V 4-pin connector:
Both these connectors must be attached.
Please explain why the FPGA image is needed and what do you plan to do with it.