I am working on the firmware for the P4080DS Expedition. I replaced the u-boot, RCW, and fman-ucode. However now the Ethernet does not work. The entire u boot prompt is attached. I can boot to the Yocto Linux but the Ethernet still does not work.
Warning: SERDES bank 2 expects reference clock 100MHz, but actual is 125MHz
Net: Fman1: Uploading microcode version 106.2.18
Could not get PHY for P4080DS_MDIO3: addr 4
Failed to connect
Fman2: Uploading microcode version 106.2.18
Could not get PHY for P4080DS_MDIO1: addr 0
Failed to connect
FM1@DTSEC2
Error: FM1@DTSEC2 address not set.
, FM1@TGEC1
Error: FM1@TGEC1 address not set.
, FM2@TGEC1
Error: FM2@TGEC1 address not set.
From this prompt I believe the problem is in the fman-ucode. Any help would be appreciated.
Thanks
James
Original Attachment has been moved to: UBoot-Log.zip
Could not get PHY for P4080DS_MDIO1: addr 0
Failed to connect
This are the Ethernet lines based on the P4080 Development System User's Guide. How do I fix this issue? Is it an RCW problem, a FMAN u-code error, or in the uboot configuration.
ethact=FM1@DTSEC2
ethprime=FM1@DTSEC1
If I set these variables and the ethaddr variables I still get the
'Could not get PHY for P4080DS_MDIO1: addr 0'
problem.
Thanks again! James
> Could not get PHY for P4080DS_MDIO3: addr 4
Check the PHY connection schematics and its configured address
> Error: FM1@DTSEC2 address not set.
It is required to define MAC addresses for the DTSECs as environment variables - example:
ethact=FM1@DTSEC1
ethaddr=00:04:9F:02:00:FD
eth1addr=00:04:9F:02:01:FD