P2020 kernel: Caused by (from MCSR=10000000): Data Cache Parity Error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

P2020 kernel: Caused by (from MCSR=10000000): Data Cache Parity Error

2,193 次查看
mlipczynski
Contributor II

CPU:P2020

OS: linux-2.6.35

Error information output from linux as below:

kernel: Machine check in kernel mode

kernel: Caused by (from MCSR=10000000): Data Cache Parity Error

 

We have this problem on 2 from few hundred boards. CPU freq is in spec, it is 1000 MHz.

What's wrong with this CPU, and how to resolve this problem?

标签 (1)
标记 (2)
0 项奖励
回复
10 回复数

2,068 次查看
mlipczynski
Contributor II

1. I don't have proper tools for swap test.

2. It is happening to an already existing board at their customer site.

0 项奖励
回复

2,066 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Why do you always repeat the same content?

Would you please provide answers for the 4 questions which I asked previously?

0 项奖励
回复

2,086 次查看
mlipczynski
Contributor II

1. No tools for that.

2. Only to already existing board at their customer site.

0 项奖励
回复

2,077 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Would you please answer the following questions?

1. Did the problem happen to only two boards?

2. How often did the failure occur?

3. how long did the board work ok before it started to fail?

4. Also would you please contract some 3rd party to do swap test for you?

0 项奖励
回复

2,117 次查看
mlipczynski
Contributor II

1. I don't have proper tools to do it.

2. It is already existing board at their customer site.

0 项奖励
回复

2,119 次查看
mlipczynski
Contributor II

1. I don't have proper tools for it.

2.  It is already existing board at their customer site.

0 项奖励
回复

2,092 次查看
yipingwang
NXP TechSupport
NXP TechSupport

I just discussed with the AE team, please refer to the following update.

Did the problem happen to only two boards?

How often did the failure occur?

how long did the board work ok before it started to fail?

 

Also would you please contract some 3rd party to do swap test for you?

0 项奖励
回复

2,167 次查看
yipingwang
NXP TechSupport
NXP TechSupport

1- does the problem follow the part or board if you do swap test?
2- have you checked [supply voltages, clock clean signals, , temperature, etc] and compared it with our RD?
3- is this an old or new design? if it is old design but new build was the cpu from new batch?

0 项奖励
回复

2,161 次查看
mlipczynski
Contributor II

1 - no swap test, not possible to be done

2 - not yet

3 - it is old design and cpu is from old batch, this device was working correctly few years, problems started now

0 项奖励
回复

2,125 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Would you please provide more information regarding the following questions from AE team?

 

1. Why not possible to do swap test?

 

2. Also is the failure happening to a new manufactured  board or to an already existing board at their customer site?

0 项奖励
回复