I am using DMA streaming API in my PCIE device driver for DMA transfers.
We use pci_dma_sync_single_for_device and pci_dma_sync_single_for_cpu to handover the buffer to device and cpu respectively. We assume that this will ensure necessary cache invalidation and flushing as per the direction of transfer.
But we still see data corruption. I tried reducing the DMA buffer size and the occurrence of the problem got delayed by 1 day. It is clearly a cache invalidation/flusing issue.
Could you please let us know the correct API usage for the architecture?
Regards
Rams
p2020 has coherent DMA and thus the DMA sync functions will not do any flushing (you should still call them, though). Check that the PCIe controller has been configured with snooping enabled.
Is there any chance that it's an ordering problem rather than coherency? Is the driver using proper I/O accessors to ensure that barriers are used? What happens if you insert manual flushing?
Hi
You had mentioned in your earlier reply that: Do you mean that it is required to have snooping enabled in both directions? Right now, the snooping is enabled from PCIe device to CPU and not from CPU -> PCIe device. Will that be an issue?
p2020 has coherent DMA and thus the DMA sync functions will not do any flushing (you should still call them, though). "Check that the PCIe controller has been configured with snooping enabled."
Is there any chance that it's an ordering problem rather than coherency? Is the driver using proper I/O accessors to ensure that barriers are used? What happens if you insert manual flushing?
Regards
Rams
In theory only the PCIe end should need to snoop. But, there have been some other chips where this was not the case, so it wouldn't hurt to try enabling snooping on the CPU side -- i.e. the M bit in the TLB entry, which in Linux can be accomplished by using an SMP kernel. Since this is a two-core chip, why aren't you already using an SMP kernel? Or if you are, what are you seeing that makes you say that snooping is not currently enabled from the CPU side?
Hi,
Sorry for the confusion. I meant the PCIE controller core of the device and not the CPU has snooping enabled for the transaction from device to cpu and no snoop enabled for the transaction from cpu to device.
Thanks
Rams
That doesn't answer my question. I only see one "snoop" setting in the PCIe controller. The PCIe device should not be caching memory (except perhaps under explicit software control), so there's nothing to snoop.
Hi,
Thanks a lot for your response.
Snooping is enabled in PCIe Controller. Regarding manual flushing of cache, clean_dcache_range or flush_dcache_range is not available for e500.
1) Could you please provide the correct API for manual flushing and invalidation of cache
2) I am not ruling our ordering problem. The driver does not use any barriers. Could you please let me know the recommended barriers which will work for p2020? I tried using wmb()/eieio()/mmiowb() before and after DMA transfer. It did not change the behaviour
Thanks
Rams
Why do you say that flush_dcache_range() and clean_dcache_range() are not available?
For a PCI driver you want to use writel()/readl(), or equivalent for other sizes. These will contain the needed barriers (a sync before all accesses, and an isync after loads).
Hi,
Thanks for the response.
Sorry, I was able to use flush_dcache_range(). I only have problems including clean_dcache_range() and invalidate_dcache_range().
When I compile the driver with clean_dcache_range(), I get a WARNING: "clean_dcache_range" undefined!
I have replaced all the iowrite32 and ioread32 with writel() and readl().
I also do flush_dcache_range() before and after DMA operations when the direction is DMA_TO_DEVICE.
i.e Prior to DMA transfer, a flush_dcache_range() after pci_map_single and Post DMA transfer a flush_dcache_range() before pci_unmap_single
I see minor improvement, the frequency of occurrence seems to be slightly reduced. But I still see the problem.
Let me know your inputs
thanks
Rams
I don't see anything in the code that would explain why you can't call clean_dcache_range() or invalidate_dcache_range() -- what kernel are you using? Though, remember that this is just for trying to figure out whether it's a cache issue. It's not a permanent solution. flush_dcache_range() should be sufficient for that purpose (and invalidate_dcache_range() can be dangerous). Since you say you still see the issue with flush_dcache_range(), it does not seem to be a cache issue.
writel() versus iowrite32() shouldn't matter.
Forgot to mention that the driver works fine on embedded ARM platform with the same PCIe device and also PC. The corruption is seen when using with P2020. That was the reason for looking into caching issues.!