P1025 QUICC engine

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P1025 QUICC engine

1,745件の閲覧回数
alexandermaslov
Contributor I

Where can I download ucode for P1025 QUICC engine? Is p1021 ucode compatible with p1025 QUICC engine?

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

1,415件の閲覧回数
alexandermaslov
Contributor I

Hi! I am trying to write a qiucc engine driver for p1025. My driver must not use dynamic memory allocation. I use NetComm Software Realease GA 4.4. The problem: 1) My soft call t_Handle QE_Config(t_QeParam *p_QeParam)

2) call QE_LoadUCodeToRam(tHandle, uint32_t*,uint32_t, uint64_t). ucode is taken from iram_Type_D_r1.h.

3) call t_Error QE_Init(t_Handle). The programm hangs in this function. It can't issue command to quicc engine, i.e. succesful return from QE_IssueCmd(p_Qe, e_QE_CMD_PROTOCOL_UNSPECIFIED, (uint32_t) p_Qe->p_QeTimerTables - pramBase).

What is the problem?

0 件の賞賛
返信

1,415件の閲覧回数
matevzlangus
Contributor III

Hi Alexander,

I can not answer your question directly, but our company can offer you help on this. We have ability to develop custom microcodes for QuiccEngine and see from the QuiccEngine side what could be the problem microcode is not responding to your commands.

best regards,

Matevz Langus

0 件の賞賛
返信

1,415件の閲覧回数
alexandermaslov
Contributor I

Thank you, Matevz! My company will think about your offer.

0 件の賞賛
返信

1,415件の閲覧回数
Pavel
NXP Employee
NXP Employee

1,415件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hi,

It can be download from Linux® SDK for QorIQ Processors|Freescale,click "SDK binary images", choose QorIQ Linux SDK v.1.6 e500v2 Image.

Login and accept online agreement, the file fsl_qe_ucode_1021_10_A.bin can be found under \p1025twr