P1010 data corruptions on 10/100Mb LAN speed in SGMII mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P1010 data corruptions on 10/100Mb LAN speed in SGMII mode

1,752 Views
serhiyhryhorchu
Contributor I

We have a custom project based on Р1010 processor with 3 network interfaces connected to PHY (Marvell 88E1112) using SGMII interface. P1010 => SGMII => 88E1112 => 10/100/1000BASE-T.

During tests we found out that when the link rate was 10/100Mb the data transmitted by the processor were corrupted while the received data were not corrupted.

When the rate was 1000Mb there were not any problems and the data were transmitted in both directions without any corruptions.

We use QorIQ SDK 1.8. We tried to use QorIQ SDK 1.9 but the result was the same.

Could you help us to find out the reasons for corruptions with data transmitted at 10/100Mb rate please.

Labels (1)
0 Kudos
Reply
1 Reply

1,565 Views
sergey_gavrish
Contributor II

It seems like i have the same problem. Proc NXP LS1012A, PHY VSC8552, SGMII MAC to 100Base-FX media. Rx packets can be received, Tx packets always stay at zero through "$ ifconfig ethX".

And there are no problem in SGMII to 1000Base-X. 

0 Kudos
Reply