Is the P1022 processor compatible with the Nand Flash which's page size is over 4KB ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is the P1022 processor compatible with the Nand Flash which's page size is over 4KB ?

671件の閲覧回数
chengliu
Contributor I

I see in the p1022rm datasheet that the p1022 is only compatible with small (512 + 16 bytes) and large (2048 + 64 bytes) page parallel NAND Flash. Thanks!

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

605件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

No, 4K page size is not supported.

605件の閲覧回数
chengliu
Contributor I

Thank you very much!

0 件の賞賛
返信