HugeTLBFS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HugeTLBFS

1,796件の閲覧回数
genuap
NXP Employee
NXP Employee

I'm considering using HugeTLBFS - I'm just wondering if anyone has implemented it before, and what your experience was.

And, as an additional question - has anyone ported it and used it under 32-bit linux?

Thanks,

Paul

タグ(2)
0 件の賞賛
3 返答(返信)

1,564件の閲覧回数
scottwood
NXP Employee
NXP Employee

HugeTLB is supported on recent 32-bit mpc85xx/QorIQ kernels, as long as you have large physical address support enabled.

0 件の賞賛

1,564件の閲覧回数
genuap
NXP Employee
NXP Employee

Thanks - what about without large phys address (i.e. only 32-bit addressing). My understanding is that the MMU code is different and unsupported. Anyone ever try it or back-port it to a strictly 32-bit machine?

Thanks,

Paul

0 件の賞賛

1,564件の閲覧回数
scottwood
NXP Employee
NXP Employee

It is not supported if large physical address support is turned off.  There should be no problem enabling large physical address support on any mpc85xx/QorIQ chip, even if the chip doesn't support 36-bit physical.  It's about Linux's internal data structures, not the hardware.

0 件の賞賛