I am looking at the possiblity of using the P1020 in a design where it uses the mode to boot directly into a eMMC device resident on the PCB. I have experience using this on an iMX6 and would like to apply it to my P1020 design.
What I do not see on the P1020 is a mode similar to the USB boot mode on the iMX6 which allows me to boot into the MFGTool to initially load the software. Is there a similar capability on the P1020?
What is usually done to perform the initial programming for a P1020 board that nominally boots from MMC?
Regards,
Doug Bailey
解決済! 解決策の投稿を見る。
Have a great day,
The P1020 has COP/JTAG interface for external debugger and can boot under debugger control while there is not any other boot device. For exampe CodeWarrior can initialize the P1020 memory, download software and start it. The P1020 SD/MMC controller is compatible with MultiMediaCard System Specification, Version 4.2. It was issued when eMMC had not introduced yet. It can boot from the MMC card or from eMMC device while treat it as MMC card.
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Have a great day,
The P1020 has COP/JTAG interface for external debugger and can boot under debugger control while there is not any other boot device. For exampe CodeWarrior can initialize the P1020 memory, download software and start it. The P1020 SD/MMC controller is compatible with MultiMediaCard System Specification, Version 4.2. It was issued when eMMC had not introduced yet. It can boot from the MMC card or from eMMC device while treat it as MMC card.
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------