Hello,
How can be calculated the MIPS/MHz ratio of the P4080 processor ? (@ 1200 or 1500 MHz)
Regards,
Tugay
解決済! 解決策の投稿を見る。
Please note that MIPS/MHz ratio is a constant.
For the e500mc core it is about 2.5 DMIPS/Mhz.
Please note that MIPS/MHz ratio is a constant.
For the e500mc core it is about 2.5 DMIPS/Mhz.
Hello,
And now two things are;
Best Regards
Tugay
1) the e500mc is capable of:
SP FP = 1 OP/cycle
DP FP = 0.5 OP/cycle
2) ECC is not implemented.
The L1 caches have:
— Instruction cache: 1 parity bit per word of instruction, 1 bit of parity per tag
— Data cache: 1 parity bit per byte of data, 1 bit of parity per tag
Refer to the e500mc Core Reference Manual:
http://cache.nxp.com/files/32bit/doc/ref_manual/E500MCRM.pdf
Hello,
Does P4080 processor support vector floating- point operations ? So , does it use AltiVec technology ?
Best Regards,
Tugay
No.
Please refer to the E500MCRM, e500mc Core Reference Manual:
http://cache.nxp.com/files/32bit/doc/ref_manual/E500MCRM.pdf