Ethenet Ping Fail issue in P1022 Uboot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethenet Ping Fail issue in P1022 Uboot

627 Views
senthil_k
Contributor I

Hi,

We are testing the ethernet interface in P1022 processor based custom board in which  eTsec interface is connected to the Marvel switch 88E6165 via RGMII interface. Ping command is getting failed when we tried to ping from board to PC in UBoot console.

ETSEC Register values are as follows,

1. Ethernet Control Register, ECNTRL (Base Addr + 0x20): 0x50

2. MAC Configuration Register 1, MACCGG1 (Base Addr + 0x500): 0xf

3. MAC Configuration Register 3, MACCGG2 (Base Addr + 0x504): 0x7205

We observed following bits in TSAT (Transmit Status Register, Base Addr + 0x104) is set during ping command,

1. Value of TSAT register while retruning from tsec_init(struct eth_device *dev, bd_t * bd) function is 0x0

2. Value of TSAT register while entering ping_send(void) function is 0x80000000 (bit Transmit halt of ring 0, THLT0 is high)

3. Value of TSAT register in ping_timeout(void) function is 0x80008000 (bit THLT0 and TXF0 are high)

4. Value of IEVENTGn (Base Address + 0x10) in ping_timeout(void) function is 0x00100000

Please let us know why THLT0 bit of TSAT register is getting set and please let us know the proper configuration details to make etsec interfcae to work in RGMII mode.

Labels (1)
0 Kudos
2 Replies

388 Views
Pavel
NXP Employee
NXP Employee

Check u-boot configuration using u-boot source code. Is u-boot on your board configured for Ethernet working in RGMII mode?

U-boot configuration file is located in the u-boot source folder: /include/configs. This folder contains the .h files for the different boards.

See documentation on the following page:

http://git.denx.de/?p=u-boot.git;a=blob_plain;f=README;hb=HEAD

and

http://www.denx.de/wiki/view/DULG/UBoot


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

388 Views
senthil_k
Contributor I

Hi Pavel,

Thanks for your response, our current issue is whenever we try ping command, RMON registers in eTSEC controller is incremented but data is not seen in the RGMII wire.

Please let us know why the packets are dropped after MAC layer and how to debug it.

RMON register value are as follows,

  1. eTSECx_TR64 (offset address 0x680, Transmit and Receive 64-byte frame counter): 2
  2. eTSECx_TBYT (offset address 0x6E0, Transmit byte counter): 0x80
  3. eTSECx_TPKT (offset address 0x6E4, Transmit packet counter): 2
  4. eTSECx_TBCA (offset address 0x6EC, Transmit broadcast packet counter): 2

We have configured in RGMII 1G mode by setting ECNTRL and MACCFG2 registers of eTSEC as follows,

1. Ethernet Control Register, ECNTRL (Base Addr + 0x20): 0x1050

2. MAC Configuration Register 2, MACCGG2 (Base Addr + 0x504): 0x7205

With Thanks and Regards,

R.Senthilkumar

0 Kudos