Hi,
We are seeing same build breakage as mentioned here:
https://lists.yoctoproject.org/pipermail/meta-freescale/2015-January/012367.html
Following is the commit probably responsible for this:
commit d7df92b6f5c1a673341d54d6b064ad2fd7b16d74
Author: Ting Liu <ting.liu at freescale.com>
Date: Wed Jan 7 17:54:59 2015 +0800
udev-extraconf: replace bbappend with own recipe
* introduce variable RULE for DPAA FMan ethernet ports name rule.
* use 72-fsl-dpaa-persistent-networking.rules for t1024, same as e6500.
Signed-off-by: Ting Liu <ting.liu at freescale.com>
An excerpt from build log:
Collected errors:
* check_data_file_clashes: Package udev-rules-qoriq wants to install file /var/arehman/mel-cedar/build_p2020rdb/tmp/work/p2020rdb-mel-linux-gnuspe/console-image/1.0-r0/rootfs/etc/udev/mount.blacklist
But that file is already provided by package * udev-extraconf
* opkg_install_cmd: Cannot install package packagegroup-base-extended.
ERROR: Function failed: do_rootfs
Note that we are on the latest meta-fsl-ppc layer: commit 060e2779783a8e581cdace77bf833e4b80f63279
Any updates on the fix?
Regards,
Abdur Rehman
解決済! 解決策の投稿を見る。
The fix for this issue has been merged in upstream. meta-fsl-ppc - Layer containing Freescale PPC hardware support metadata
Thanks for the support
What command sequence is used for SDK building?
Is Ubuntu operation system is used for SDK?
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
The fix for this issue has been merged in upstream. meta-fsl-ppc - Layer containing Freescale PPC hardware support metadata
Thanks for the support