How to add gcc and g++ to custom minimal image, I've tried to add:
IMAGE_INSTALL_append = " sqlite3 gcc g++ make"
into local.conf. Make is found, however, gcc and g++ are not, why?
Here is also bblayers.conf:
# LAYER_CONF_VERSION is increased each time build/conf/bblayers.conf
# changes incompatibly
LCONF_VERSION = "6"BBPATH = "${TOPDIR}"
BBFILES ?= ""BBLAYERS ?= " \
/home/testuser/QorIQ-SDK-V1.9-20151210-yocto/sources/poky/meta \
/home/testuser/QorIQ-SDK-V1.9-20151210-yocto/sources/poky/meta-yocto \
/home/testuser/QorIQ-SDK-V1.9-20151210-yocto/sources/poky/meta-yocto-bsp \
/home/testuser/QorIQ-SDK-V1.9-20151210-yocto/sources/meta-openembedded/meta-oe \
/home/testuser/QorIQ-SDK-V1.9-20151210-yocto/sources/meta-openembedded/meta-networking \
/home/testuser/QorIQ-SDK-V1.9-20151210-yocto/sources/meta-openembedded/meta-perl \
/home/testuser/QorIQ-SDK-V1.9-20151210-yocto/sources/meta-openembedded/meta-python \
/home/testuser/QorIQ-SDK-V1.9-20151210-yocto/sources/meta-openembedded/meta-ruby \
/home/testuser/QorIQ-SDK-V1.9-20151210-yocto/sources/meta-openembedded/toolchain-layer \
/home/testuser/QorIQ-SDK-V1.9-20151210-yocto/sources/meta-freescale \
/home/testuser/QorIQ-SDK-V1.9-20151210-yocto/sources/meta-freescale-internal \
/home/testuser/QorIQ-SDK-V1.9-20151210-yocto/sources/meta-freescale-extra \
"
BBLAYERS_NON_REMOVABLE ?= " \
/home/testuser/QorIQ-SDK-V1.9-20151210-yocto/sources/poky/meta \
/home/testuser/QorIQ-SDK-V1.9-20151210-yocto/sources/poky/meta-yocto \
"
解決済! 解決策の投稿を見る。
The toolchain runs on target board, which is the same exact version as the cross tools in this SDK, is only included in
fsl-image-full rootfs, if you want to add toolchain into other rootfs images, do the following:
1. Edit fsl-image-minimal.bb/fsl-image-core.bb to add packagegroup-core-buildessential in the IMAGE_INSTALL
variable.
2. $ bitbake <rootfs-target>.
Please try the following:
Please add "IMAGE_INSTALL +=packagegroup-core-buildessential" in sources/meta-freescale/recipes-fsl/images/fsl-image-minimal.bb, and rebuild minimal rootfs filesytem with "$bitbake fsl-image-minimal"
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
The toolchain runs on target board, which is the same exact version as the cross tools in this SDK, is only included in
fsl-image-full rootfs, if you want to add toolchain into other rootfs images, do the following:
1. Edit fsl-image-minimal.bb/fsl-image-core.bb to add packagegroup-core-buildessential in the IMAGE_INSTALL
variable.
2. $ bitbake <rootfs-target>.
Please try the following:
Please add "IMAGE_INSTALL +=packagegroup-core-buildessential" in sources/meta-freescale/recipes-fsl/images/fsl-image-minimal.bb, and rebuild minimal rootfs filesytem with "$bitbake fsl-image-minimal"
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------