Mostly that, what are the considerations to take when soldering this chip, whats the recomended process and materials to do so?
Hello, We are using the XSON3. I was also wondering what is the best way to connect the chip to the antenna, we are currently using a 2x4 mm pcb with the biggest posible traces width, is there a recomended pcb layout or different recomended material?
Please check the following application note
https://www.nxp.com/docs/en/application-note/AN162910.pdf
I hope this will help you.
Can you tell me the package that you are using, is your are using the XSON3, it can support 260 C as package body temperature as is shown here
Regards
Vicente