Hi,
I install Platform_Software_Integration_S32R45_2022_03.exe, and import "Bootloader_S32R45_ASR_4.4_M7" project to EB.
Then, i add "Spi" module to the project, and generate project.
When configure "Config Variant" is "VariantPostBuild", the Bootloader.bin can load and run M7 app.
But, configure "Config Variant" is "VariantPreCompile", the Bootloader.bin can't load and run M7 app, it occur "hard fault", enter "HardFault_Handler", then enter "MemManage_Handler".
Why does it occur "hard fault"? And, how to solve it?
Best regards!