tcp/ip stack(lwip) integration on EVB of S32R41

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

tcp/ip stack(lwip) integration on EVB of S32R41

235 Views
yuran
Contributor II

Hi All,

I'm using the evaluation board of S32R41,trying to integrate the tcp/ip stack (lwip)。Refering to NXP's demo "lwip_S32R41_NXP_RTOS_M7_0",I configure GMAC and lwip stack on core M7_1 in  another demo project called "S32R41+TEF82xx_Development_Platform"。However,the result is not as expected,failure for ping。The code get stuck in the function "gmacif_low_level_output",and GMAC TX/RX interrupt handdle can not be triggered。I have no idea what needs to be concerned,anyone can help with it ?

yuran_0-1700882557726.png

 

0 Kudos
Reply
1 Reply

206 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

unfortunately the RADAR application support is limited and the team is not answering on communities.

This looks like application issue. Could you submit the ticket at NXP.com so your question will reach the team.

Best regards,

Peter

0 Kudos
Reply