tcp/ip stack(lwip) integration on EVB of S32R41

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

tcp/ip stack(lwip) integration on EVB of S32R41

192 次查看
yuran
Contributor II

Hi All,

I'm using the evaluation board of S32R41,trying to integrate the tcp/ip stack (lwip)。Refering to NXP's demo "lwip_S32R41_NXP_RTOS_M7_0",I configure GMAC and lwip stack on core M7_1 in  another demo project called "S32R41+TEF82xx_Development_Platform"。However,the result is not as expected,failure for ping。The code get stuck in the function "gmacif_low_level_output",and GMAC TX/RX interrupt handdle can not be triggered。I have no idea what needs to be concerned,anyone can help with it ?

yuran_0-1700882557726.png

 

0 项奖励
回复
1 回复

163 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

unfortunately the RADAR application support is limited and the team is not answering on communities.

This looks like application issue. Could you submit the ticket at NXP.com so your question will reach the team.

Best regards,

Peter

0 项奖励
回复