sja1105q rgmii mode port 1 sometimes cannot send packet but it can receive packets

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

sja1105q rgmii mode port 1 sometimes cannot send packet but it can receive packets

177 次查看
jasonmuscle
Contributor I

sja1105q is normal most of the time, but occasionally the device connected to port 1 can not receive data, but the data can be sent, that is, port 1 can not send data, read RGMII_TX_CLK_1 reg 0x10001C is now 0x0B000800, the value is correct, Re-manually write register RGMII_TX_CLK_1 to the same value, the communication is normal, what is the situation that causes this? What can be done to prevent this from happening by accident

标记 (1)
0 项奖励
回复
0 回复数