sja1105q rgmii mode port 1 sometimes cannot send packet but it can receive packets

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

sja1105q rgmii mode port 1 sometimes cannot send packet but it can receive packets

176 Views
jasonmuscle
Contributor I

sja1105q is normal most of the time, but occasionally the device connected to port 1 can not receive data, but the data can be sent, that is, port 1 can not send data, read RGMII_TX_CLK_1 reg 0x10001C is now 0x0B000800, the value is correct, Re-manually write register RGMII_TX_CLK_1 to the same value, the communication is normal, what is the situation that causes this? What can be done to prevent this from happening by accident

Tags (1)
0 Kudos
Reply
0 Replies