sja1105q rgmii mode port 1 sometimes cannot send packet but it can receive packets

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

sja1105q rgmii mode port 1 sometimes cannot send packet but it can receive packets

189件の閲覧回数
jasonmuscle
Contributor I

sja1105q is normal most of the time, but occasionally the device connected to port 1 can not receive data, but the data can be sent, that is, port 1 can not send data, read RGMII_TX_CLK_1 reg 0x10001C is now 0x0B000800, the value is correct, Re-manually write register RGMII_TX_CLK_1 to the same value, the communication is normal, what is the situation that causes this? What can be done to prevent this from happening by accident

タグ(1)
0 件の賞賛
返信
0 返答(返信)