sc18is602b What is the reset requirement?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

sc18is602b What is the reset requirement?

454 次查看
obroad
Contributor II

One demonstration circuit I've looked at shows the reset signal coming from the host microcontroller, which seems like a waste of an I/O pin.

Another appears to show an RC network, values unclear.

If I don't actually want the microcontroller to force reset the device then can I just tie reset high, is an RC delay enough, or would the device need a clean reset signal from a voltage monitor? With some other devices (Microchip I/O expanders) the reset appears optional and can be tied high.

I see that the reset pulse latches the state of the address pins. This would imply that reset timing is important.

标签 (1)
0 项奖励
1 回复

399 次查看
reyes
NXP TechSupport
NXP TechSupport

Hi,

There is an on-chip reset circuit after the power is on.
You don’t have to drive the reset pin unless you want to reset the device manually. 

Regards,

Jose

NXP Semiconductors

0 项奖励