read access issue about sja1105qel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

read access issue about sja1105qel

Jump to solution
2,387 Views
SungBong
Contributor II

Hi. 

Our system uses SJA1105QEL ethernet switch (Host is MPC5748G).

I want to read configuration value. so i tried to access address 0x00000000 (ETH_DYN 0x00h) but the result of read access is same as write access (SDO is mirrored as SDI).

According to the software manual, i understand that first 32 bits are access control value and next 32 bits are ignored value for reading data.

So, i tested following method in S32 project.

 

 -test code

image.png

 
 
 
 

-result 

image.png

Do you think this method is wrong or other problem exists?

please any help for me.

 

best regards.

thank you.

Labels (1)
0 Kudos
1 Solution
2,338 Views
guoweisun
NXP TechSupport
NXP TechSupport

guoweisun_0-1602487293154.png

Refer to this timing format!

 

View solution in original post

10 Replies
2,359 Views
guoweisun
NXP TechSupport
NXP TechSupport

Suggest to write this register firstly then read it to verify the content.

0 Kudos
2,358 Views
SungBong
Contributor II

Dear guoweisun.

i already wrote static configuration data such as below before read access.

image.png

image.png

 

do i need anything else?

 

best regards.

0 Kudos
2,350 Views
guoweisun
NXP TechSupport
NXP TechSupport

You can read your written content now?

 

0 Kudos
2,344 Views
SungBong
Contributor II

where write access, the data is transmitted via SDO. 

i can read buffer after write access.

buffer has mirroring data from SDO same as SDI.

0 Kudos
2,339 Views
guoweisun
NXP TechSupport
NXP TechSupport

guoweisun_0-1602487293154.png

Refer to this timing format!

 

2,325 Views
guoweisun
NXP TechSupport
NXP TechSupport

Yes,please follow the timing !

 

0 Kudos
2,289 Views
SungBong
Contributor II

I solved this issue.

i think it was SS signal problem.

i should have checked Continous SS option in S32DS.

thank you for your help a lot.

best regards.

0 Kudos
2,333 Views
SungBong
Contributor II

you mean i need to insert delay time between first 32 bits and second 32 bits for t3?

0 Kudos
2,370 Views
guoweisun
NXP TechSupport
NXP TechSupport

Data (containing the number of 32-bit quadlets to be read and address to read from) is
received on the SDI input of the switch and is treated as a sequence of 32-bit quadlets.
Data corresponding to the address received is output on SDO pin of the switch.

2,367 Views
SungBong
Contributor II

Dear guoweisun.

thank you for your reply.

In my case, i want to read a register value at 0x00. 

Where read access, i understand first 32 bits are mirrored same data via SDO.

I expect to read next not mirrored 32 bits data via SDO. but the next 32 bits are also mirrored SDI data. 

i think it is something wrong.

is my test code wrong or not?

 

best regards.

0 Kudos