pn5180 JCOP MIFARE APP Auth doesn't work

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

pn5180 JCOP MIFARE APP Auth doesn't work

115件の閲覧回数
jekim0109
Contributor II

Hello, I'm Jay.

There is a JCOP card ((SAK-0x28) Type A - Layer 3) using pn5180 and linux library sw352236.

Inside the JCOP card are the MIFARE App and Type A Layer 4 App. Among them, I tried Auth to use the MIFARE App, but Timeout occurs. (The same should not be done even if you maximize the MIF_AUTH_TIME value.)

For your information, I used Nfcrlib_SimplifiedAPI_ISO among the samples.

wStatus = phhalHw_Exchange(
    gphNfcLib_Params.sDiscLoop.pHalDataParams,
    PH_EXCHANGE_DEFAULT,
    (uint8_t *)(((phNfcLib_Transmit_t *)pTxBuffer)->phNfcLib_RawTransmit.pBuffer),
    wTxBufferLength,
   &gphNfcLib_State.pRxBuffer,
   &gphNfcLib_State.wRxLength
);

 

 

タグ(2)
0 件の賞賛
1 返信

99件の閲覧回数
Fabian_R
NXP TechSupport
NXP TechSupport

Hello sir,

Thank you very much for using our products. Unfortunately, I cannot provide support for JCOP products since they are secured products. Please contact your nearest Distributor or, in case you are already working with someone directly from NXP contact them.

I'm very sorry for the inconvenience.

Best Regards,
Fabian
0 件の賞賛