openssl SEC hardware offload LSDK 21.08

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

openssl SEC hardware offload LSDK 21.08

455 次查看
NaveenS11
Contributor I

In the following page. I am doing manual build. https://www.nxp.com/docs/en/user-guide/LSDKUG_Rev21.08.pdf

while building cryptodev-linux the first error which I got

user@localhost:~/cryptodev-linux$ make
make -C /lib/modules/5.10.35-dirty/build M=/home/user/cryptodev-linux modules
make[1]: *** /lib/modules/5.10.35-dirty/build: No such file or directory. Stop.
make: *** [Makefile:27: build] Error 2
user@localhost:~/cryptodev-linux$

so , i installed following .deb package i installed 

dpkg -i linux-headers-5.10.35-dirty_5.10.35-dirty-4_arm64.deb 

after, installing the package I am getting following error.

user@localhost:~/cryptodev-linux$ make
make -C /lib/modules/5.10.35-dirty/build M=/home/user/cryptodev-linux modules
make[1]: Entering directory '/usr/src/linux-headers-5.10.35-dirty'
CC [M] /home/user/cryptodev-linux/ioctl.o
/bin/sh: 1: scripts/basic/fixdep: Exec format error
make[2]: *** [scripts/Makefile.build:279: /home/user/cryptodev-linux/ioctl.o] Error 2
make[2]: *** Deleting file '/home/user/cryptodev-linux/ioctl.o'
make[1]: *** [Makefile:1821: /home/user/cryptodev-linux] Error 2
make[1]: Leaving directory '/usr/src/linux-headers-5.10.35-dirty'
make: *** [Makefile:27: build] Error 2

can anyone help me on this!!

0 项奖励
回复
1 回复

445 次查看
NaveenS11
Contributor I

the default lsdk21.08 have a openssl software. but when ever I try to run openssl getting following error

openssl: symbol lookup error: openssl: undefined symbol: EVP_mdc2, version OPENSSL_1_1_0

0 项奖励
回复